AXIS#.PL.MODPEN

Description

A value of 0 disables the modulo-position and a value of 1 enables the modulo-position feature. The modulo-position feature can be used for circular applications such as round tables.

The position loop of the drive uses a linear position variable but the data-exchange between the user and the drive uses the modulo-position calculation in order to convert values from linear format into modulo format and vice versa.

The following figure shows the interface between the user and the drive for AXIS#.PL.MODPEN=1:

Examples

Code

Axis 1 position is modulo’d to 0-360 where MODP1 is beginning of range and MODP2 is the end of range.

-->AXIS1.PL.FB
500.000 [deg]
-->AXIS1.PL.MODP1 0
-->AXIS1.PL.MODP2 360
-->AXIS1.PL.MODPEN 1
-->AXIS1.PL.FB
140.000 [deg]

Context

For more information see Modulo Position .

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

AXIS#.PL.MODP1, AXIS#.PL.MODP2
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
AXIS1.PL.MODPEN

500ch

0bh

Unsigned8

-

-

Read/Write

No

AXIS2.PL.MODPEN

510ch

0bh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.MODPEN

5912

1718

Unsigned8

Read/Write

-

AXIS2.PL.MODPEN

71448

1171

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.MODPEN

5912

Unsigned8

Read/Write

-